Section 1: Registration on the “myNORD” internet portal
(1) The “https://shop.nord.com” internet portal (hereinafter referred to as NORD portal) is aimed at non-registered as well as at registered users.
(2) Users as referred to in these terms of use are exclusively companies within the context of art. I.1, 1° Economic Law Code (“Wetboek Economisch Recht”, “WER”) (that is natural or legalentities or partnerships having legal status that upon closing a legal transaction do business in the pursuit of their commercial or independent activities), legal entities under public law or special funds under public law.
(3) All users can use the NORD portal to find out more about our products, to configure them, to edit their configurations, to save and to print them. Registered users may use the “Configure” or “Configuration” button to create an offer request. By further clicking the “Create new configuration” button, they may add products to this offer request, optionally using the configurator. A completed offer request is saved in a project list. Offer requests created this way remain non-binding and do not represent a contract offer by the customer.
(4) Furthermore, after the integration of the NORD DRIVESYSTEMS E-SHOP (hereinafter referred to as e-shop) into the NORD portal, all users can obtain information about the spareparts for the drive they are interested in as well as about other products from NORD. Registered users can also order them quickly and easily.
(5) Users may request their registration via our online registration form with truthful statement of name and surname, company, e-mail address, telephone number, address and, if available and known, the company’s customer number at NORD and the VAT number, as well as an individual, freely selectable password. Afterwards, the user receives a confirmation of receipt by e-mail to the specified e-mail address including a confirmation link. After the user has confirmed this confirmation link, we will check the provided information for the purpose of an account activation. As soon as we have activated the account, the user receives another email to the specified e-mail address. After usage of the login data and the password, the user is a registered user and can complementarily use the e-shop for order processes. Registered users must inform us immediately about later changes to their information.
(6) Users have no right to their registration. Furthermore, we are entitled to rescind a granted registration if we discover that the user provided incomplete or wrong data for the registration or violates these terms of use. We reserve the right to check the usage authorisation by sending another confirmation e-mail.
(7) Registered users must maintain secrecy about their login data, especially the password.
(8) The user data required for registration are collected and can be submitted, for example, to transport companies and/or financial service providers as far as this is necessary for the execution of an order. The user hereby expressly agrees to this data transfer.