NORD DRIVESYSTEMS - NORD CON





NORD CON NORD CON

release 1.25
release 1.25

This software now works under Windows 95, 98, 2000 and XP.

  • Download the below file, and unzip the file using Winzip or an other unzip tool.
  • Run the Setup program from the folder DISK1 and follow the instructions.
  • Please find in the readme file, which you will find at the end of the installation, the changes from the newest release.

download

NORD CON 1.25 Download (ca. 12 MB)

The version contains the configuration for the NORDAC frequency inverter trio SK 300E, SK 500E, vector mc, SK 700E and vector.

System requirements:

IBM or compatible PC, Pentium or similar processor 32 Megabyte RAM Windows 95, 98, 2000, ME, XP 15 MB free hard disk space, super VGA graphic ( 800x600 ), mouse.

Disclaimer

Getriebebau NORD is not liable for damages resulting form the use of this software, even if Getriebebau NORD has been informed about the possibility of such damages.

Sales contactSales contact

Locatortool
Find distributors and sales people