Keyword search | Sales contact
Sales contact
Phone: 888-314-6673
Find current News articles and pictures of our company and products, as well as information on upcoming and past trade fairs.
NORD expands headquarters and creates 100 new jobs NORD's headquarters facilities in Bargteheide near Hamburg, Germany, are currently being extended, with plans to increase the location’s floor space from 31,300 m² to 52,000 m² by 2009.
Introducing the decentral SK 2xxE: Integrated drive units for price-sensitive applications NORD extends the flexible NORDAC DA series of decentral drive components, adding the new type SK 2xxE frequency inverters which were first presented at this year's Hannover Messe trade show.
Energy-saving inverters with magnetization adjustment option More efficient operation of AS motors with optimized motor current SK 5xxE and SK 700E type frequency inverters can save re-sources by automatically reducing the magnetization of an asynchronous motor when the motor is operated under partial load. The motor current is thereby adjusted as needed, and heat losses are minimized.
Expertise for energy-efficient drives: Three ways to ensure optimal savings Success in developing highly efficient drives depends on seizing energy saving potentials in gearboxes, motors and power electronics alike. NORD has been following this integrated approach since the mid-1990s in all efforts to supply drive units with optimized overall efficiency.
Optimized for high loads: Powerful helical bevel geared motors in an FEM-calculated housing The UNICASE housings of NORD's new three-stage type SK 9096.1 helical bevel geared motors have been optimized through FEM calculations, ensuring cost-efficient production and high load capacity.
Growing family of SK 5xxE frequency inverters: Extended model range now consists of six sizes NORD has extended its SK 5xxE line of frequency inverters by new size 5 and 6 models. Thereby, new performance ranges have been added: in addition to the former 0.25 to 7.5 range, users can now also choose inverters up to 22 kW.
Ethernet connection for NORD frequency inverters NORD offers new solutions for the growing number of drive system users who are choosing Ethernet-based fieldbus connections for automation tasks.
Cost-efficient drive solutions for hazardous areas with Ex e motors certified for inverter operation Gas explosion-protected drives in “increased safety” (Ex e) from NORD are blanket approved for operation with a frequency inverter. Users can thus tap high savings potentials:
Giants in a UNICASE housing: New industrial gear units with max. torques up to 200,000 Nm NORD has extended its range of industrial gear units, adding new models with maximum torques of 60,000 Nm, 90,000 Nm, 135,000 Nm and 200,000 Nm. NORD is the only supplier worldwide to construct even 90,000 Nm and beyond models according to the proven UNICASE concept.
Safety first: NORD frequency inverters feature Many machines and plants, e.g. machine tools such as milling machines, need to fulfill strict operator safety standards: when a safety circuit is activated, operators must be safe from rotating machine parts.
Fieldbus connection options: NORD frequency inverters support Ethernet NORD Drivesystems, a full-line supplier for drive technology, offers the NORDAC SK 5xxE and SK 700E inverter series which cover the complete spectrum of standard, enclosure-mounted intelligent frequency inverters.
Full-line service provider for drive technology NORD Drivesystems, founded in 1965 in Bargteheide near Hamburg, Germany, manufactures and distributes mechanical and electronic drive technology.
Eco-friendly and cost-saving: Energy efficient drives from NORD NORD provides solutions for the power transmission industry consisting of gear reducers, motors and intelligent electronics controllers which optimize system energy efficiency.
Increased safety (Ex e) protection for inverter-controlled motors enables more cost-efficient, lighter ATEX drive solutions NORD has expanded its ATEX product lineup to include a new area of application: gas explosion-protected drives featuring “increased safety” (Ex e) which are generally approved for speed-controlled operation with a frequency inverter.
Universally applicable: NORDAC SK 700E NORD’s SK 700E frequency inverters, which belong to the tried-and-tested NORDAC line, are specified for a mid-to-upper level power range between 1,5 and 160 kW.
New Large Gearbox Assembly and Paint Booth Expansion. Since the 40,000 square foot expansion in Waunakee, WI completed in October 2006, NORD Gear has made a number of changes to increase our overall capacity and to better service customers.
New SCP Screw Conveyor Package NORD has enhanced the Clincher™ offset parallel line of gearmotors and speed reducers to include the new SCP screw conveyor package.
NORDAC SK 500E/520E/530E: Compact frequency inverters for a wide range of applications The compact frequency inverters NORDAC SK 500E/520E/530E come with a wide range of basic features and can be easily adapted to specific applications.
NORDAC DA: system components for decentral drive solutions Decentral drive technology simplifies the layout of plants and minimizes the required space and expenses. NORD has developed the flexible NORDAC DA decentral drive concept which serves to relocate electronic control technology from control cabinets directly to the drive.
NORDAC DA: system components for decentral drive solutions Decentral drive technology simplifies the layout of plants and minimizes the required space and expenses.
Stronger, lighter, more compact: New NORDBLOC type geared motors NORD Gear has enhanced its compact line of UNICASE geared motors through design improvements.
Easy position control with NORD frequency inverters NORD's standard asynchronous motors and frequency inverters allow for the quick and cost-efficient implementation of applications requiring relative or absolute position control (e.g. rotary tables, linear travel axes or synchronous speed control).