Frequency inverter: installation in the control cabinet or decentralised in the field?

Frequency inverters enable flexible speed control and are therefore an essential component of automated production concepts. Frequency inverters can be installed both in the control cabinet and directly on or close to the motor. What is difference between the two strategies? What are the advantages of decentralisation? Which drive concept is suitable for which application? Answers, solutions and perspectives.

One thing right away: there is usually no definite solution – too many factors play a role when choosing the drive concept. Control cabinet installation, decentralised use in the field or a combination of both? Each strategy has its advantages and disadvantages. In many cases, the placement of the frequency inverters is therefore a matter of weighing up. However, there are of course various criteria that can help in the decision-making process. In this blog post, we provide you with an overview of the different options and tell you about what you should consider when dealing with frequency inverters. Our experts in the field of drive electronics will be glad to assist you. Contact us!

Where does the frequency inverter go?
Typically, there are differences in terms of equipment, function and performance between decentralised and frequency inverters in the control cabinet. While control cabinet inverters offer the full range of functions, decentralised inverters are often simpler, stripped-down variants with a smaller range of functions. NORD DRIVESYSTEMS chooses a different path. Contrary to the common practice in the market environment, the North German drive specialist uses the same platform concept for control cabinet inverters and decentralised solutions. The result: the same level of performance and functionality regardless of the installation location.
However, the performance scope of the frequency inverter is not the sole decisive factor for or against a control cabinet installation. Aspects such as system structure, installation environment, efficiency requirements, maintenance needs and customisation options also make a difference and should be included in the considerations. The decision is often cost-driven. Ultimately, however, the drive concept should always be determined by the application requirements.
Important factors for the choice of the frequency inverter:
- Application
- Industry
- System structure
- Motor powers
- Function range
- Ambient conditions
- Maintenance effort
- Flexibility
The classic: control cabinet inverter
Traditionally, all electrical and electronic components of a system – and thus also the frequency inverters – are housed in a control cabinet. It protects both the sensitive electronics inside and the external production environment. Dirt, dust, heat, humidity and electromagnetic influences cannot enter and electromagnetic emissions, dangerous voltages or possibly occurring fires cannot get outside.
In general, the drive electronics are located in the control cabinet in 80 percent of all applications. This control architecture is particularly dominant in mechanical engineering. In most cases, the spatial separation of motor and control technology has historical reasons, but in certain applications it is also advantageous – particularly when it comes to high powers and extreme environmental conditions. Although decentralised drive systems are common for the explosion hazard areas of zone 22 (explosive dusts), explosive gases, mists and vapours require such high protective measures that decentralisation is technically possible but would not make sense in terms of economic efficiency. Sensitive areas such as the process industry, the chemical industry and painting tasks therefore use an installation point in the control cabinet in most cases. In some applications, it may also be necessary to have central access to the frequency inverters.
With these requirements, installation in the control cabinet makes sense:
- High powers
- Extreme ambient conditions such as explosive gases, mists and vapours
- High hygienic requirements
- Central frequency inverter access required
The future belongs to decentralised frequency inverters
In many places, the control cabinet is still considered the ultimate solution for housing frequency inverters – it is uncertain whether this remains the case in the future. For in general, an increasing system concept can be observed; decentralised automation concepts are gaining ground. Wherever possible, users are resorting to solutions that are distributed in the system – driven by the shift towards modular production plants and the increasing demand for compact, service-friendly and economic drives. Europe is leading the way, but the USA and Asia are following suit. In particular, sectors such as intralogistics, conveyor technology, the food industry, airport technology and the packaging industry are increasingly relying on decentralised concepts with frequency inverters installed on or close to the motor. This is not surprising, because the specific advantages of decentralised drive technology come into effect particularly with extensive plants as well as in modular and mobiles systems.
Decentralisation means that the drive tasks are distributed to individual, intelligent components in the field. They are installed where they are needed – i.e. on or close to the motor. Decentralisation of drive technology is primarily used in the lower and middle power range and enables a system design that consists of autonomous production islands that largely regulate their processes themselves. This reduces the load on the higher level control system and decreases system complexity. For the user, this means faster commissioning and simplified maintenance and repair processes. With a modular concept there is also maximum flexibility, as changes to the system architecture can be made at any time without large structural modifications. As a result, this means: reduced costs and more efficiency.
Advantages of decentralisation
The decentralised automation concept leads to a more cost-effective and uncomplicated control cabinet construction. If the frequency inverters are installed directly in the field, less space is required in the control cabinet. Consequently, the control cabinet can be smaller or may even be eliminated entirely. As there is no frequency inverter as an extra source of heat in the control cabinet, costs for air conditioning are also reduced. This in turn has a positive effect on the energy balance.
Thanks to spatial proximity of motor and frequency inverter, both the wiring effort and the cabling between cabinet and drive in the system field are also reduced to a minimum. The advantage here is that decentralised solutions are often available as plug-in versions. This further simplifies the installation. No or only short cables are required, which – thanks to the optimal EMC properties of motor-mounted frequency inverters – do not necessarily have to be shielded. Although shielded cables cannot be dispensed with an installation close to the motor, they can be very short and are therefore cost-effective. Since the frequency inverters are mounted directly on the motor or in its immediate vicinity, commissioning close to the motor is also possible. As the connections for the power supply and the bus system are usually pluggable and looped through, this can be carried out quickly and easily – quite in contrast to star-shaped point-to-point wiring in the control cabinet. This reduces the costs.
Advantages of decentralised frequency inverters:
- Control cabinet may be smaller
- Minimal wiring and cabling work
- Simple maintenance
- Rapid commissioning thanks to pre-configuration at the factory
- Modifications and extensions to the system design easily possible at any time
- Reduced costs for the plant design
- Reduces the complexity of the system
- Increases the efficiency of the entire drive system
- Can be integrated into all automation architectures

Pioneer of innovative inverter technology
For more than 40 years, NORD DRIVESYSTEMS has been developing and producing electronic drive technology and is one of the pioneers in innovative inverter technology. The portfolio includes motor starters, frequency inverters and decentralised drive electronics such as frequency inverters up to 22 kW and motor starters up to 7.5 kW as well as frequency inverters for control cabinet installation up to 160 kW – characterised by scalable functions, high precision regulation, easy installation and operation. Different power classes, mounting options and communication modules ensure integration into all control architectures.
NORD manufactures all frequency inverters in its own factory in the East Frisian town of Aurich (Lower Saxony). The automated and flexible production structure is state-of-the-art and allows any size of order to be processed in the same manner. Even small batch sizes are possible thanks to flexible production. In 2022, 185,000 units left the factory, and the trend increases. The demand for customised drive electronics in particular is increasingly strong. To optimally meet the growing demand, NORD invested 2.5 million Euro in the site last year and expanded the production area to 7,000 m2 and the production capacity to 400,000 units.

Frequency inverters from NORD: scalable, powerful, future-proof
Whether a control cabinet inverter or a decentralised variant for use in the field. With its NORDAC product family, NORD DRIVESYSTEMS offers electronic drive technology for almost every application. The system-wide compatibility of the entire product family warrants a comparable function range, uniform operability, and common options for all NORD frequency inverters. The devices are scalable with regard to function and configuration, and can be flexibly adjusted to any application. They are quick to install, easy to operate and compatible with all common bus systems and controls. Useful features like the PLC functionality for drive-integrated functions, an energy-saving function for partial load operation, the POSICON positioning control, integrated brake choppers for 4-quadrant operation, functional safety with STO and SS1 as well as Profisafe also for motion-related functional safety tasks ensure high functional use. The frequency inverters perform open-loop or closed-loop, and are designed for operation with asynchronous and synchronous motors. The precise current vector control ensures optimal torque in a wide variety of load and speed situations. Additionally, they can take up and autonomously control many functions. In this way, the geared motor is capable of performing functions such as lifting gear, positioning, sequence control, flying saw and synchronised movement. The modular construction kit opens the door to many plug-and-play extensions and options. NORD offers innovative solutions for Ex environments with ATEX 3D.
Frequency inverters from NORD have condition monitoring solutions for predictive maintenance systems and are well equipped for use in IIoT and Industry 4.0. The integrated PLC can process data from connected sensors and actuators, initiate control sequences and communicate with other system components. The periodic or continuous recording of drive and status data allows for an early detection and avoidance of impermissible operating states. Unscheduled downtimes can be significantly reduced and status-oriented maintenance (predictive maintenance) replaces time-based maintenance. Machinery and plant downtimes can be scheduled.
Frequency inverters for any drive application:
- Integrated PLC
- POSICON positioning module
- Lifting gear function
- On-board brake chopper and braking resistor
- Closed-loop operation with incremental encoder and/or absolute encoder
- Functional safety
- Energy-saving function for partial load range
- Support of all common field bus and Ethernet dialects
- Operation of synchronous and asynchronous motors
- Protection class IP55 / IP66
- All relevant international certifications for global use
Decentralised frequency inverters in combination with control cabinet inverters
Control cabinet inverter or decentralised frequency inverter? The question suggests that these are two opposing strategies that categorically exclude each other. But this not the case at all. Quite the opposite. In many cases, a combination of both drive concepts is a sensible solution. Bottling systems in the beverage industry are a good example for such mixed concepts, i.e. the coexistence and interaction of control cabinet and decentralised technology. Where work is carried out directly with the product and corresponding hygiene standards have to be met, a control cabinet solution may be recommended. However, decentralised solutions are usually the better choice for the conveyor belts between the individual stations. Thanks to the platform concept, NORD DRIVESYSTEMS is also able to provide suitable drive solutions for these requirements with a combination of control cabinet and decentralised frequency inverters. There are no differences between the control cabinets and decentralised inverters in the field in terms of performance, communication, control and parameterisation.