News –

How NORD solutions intelligently control movements

With its drive electronics, the system supplier demonstrates its solution expertise also in the fields, where movements must be intelligently controlled. These can be found in various applications, which also have an influence on daily life.

Bargteheide, 2024-12-05

One example is the safe and efficient cutting of food products such as bread, meat or cheese. In cutting machines, the freely programmable PLC, integrated in all NORDAC frequency inverters ensures the finely tuned contact pressure of the food product. This ensures consistent precise cutting quality.

Intelligent control functions master industry-specific drive applications

When it comes to bottling liquid food products, speed is an essential factor. NORD frequency inverters ideally meet the great demands on precise speed control. They thus ensure an optimally balanced production process. Furthermore, for example, the NORDAC PRO control cabinet inverter can be integrated via Ethernet. It thereby allows for the remote maintenance of the system, with which NORD ensures high system reliability.

Drive solutions from NORD also take effect when it comes to precise positioning tasks. Here, the company offers its integrated POSICON, module, which, for example, is contained in frequency inverters such as NORDAC PRO. It allows automatic positioning control for different applications such as travelling theatre sceneries for trouble-free theatre performances.

Extensive modular range of products meets industry expertise

Solution provider NORD DRIVESYSTEMS develops and manufactures application-specific drive systems from a single source . For that, the company is using its industry expertise with which it supports customers in about 100 industries. The extensive range of modular products consisting of gear units, motors and electronic drive technology forms the basis for the implementation of solutions.

Find out more now!