News –
DuoDrive geared motor is now patented
The fewer interfaces, the higher the system efficiency – based on this maxim, NORD DRIVESYSTEMS introduced a revolutionary geared motor in a hygienic wash-down design one year ago, where the especially energy-efficient IE5+ permanent magnet synchronous motor and a single-stage helical gear unit are installed in one single housing.
Bargteheide, 2022-03-01
The completely new, compact design with full integration of motor and gear unit in one single housing is an extraordinary leap in the development of geared motors and has now been successfully patented. The long-term durability and reliability of the innovative solution in terms of design and materials has been successfully proven in months of testing during the development of the DuoDrive, and thus real pioneering work has been accomplished in the field of geared motors. The integration has been decisively advanced to achieve an optimal utilisation of installation space. Along with the IE5+ motor on which it is based, the encoder, speed feedback and brake are all safely accommodated in the housing. In addition to the high system efficiency, the smooth, unventilated and compact design, and the quiet running with minimum noise emissions are further important features of the new DuoDrive geared motor. Elimination of many wearing parts results in lower maintenance.