News –
How NORD solutions intelligently control movements
Drive electronics from NORD DRIVESYSTEMS is the key to any drive application. With its
NORDAC frequency inverters
, the system supplier demonstrates its solution expertise also in the fields, where movements must be intelligently controlled. These can be found in various applications, which also have an influence on daily life.
Brampton, ON, 2024-12-05
One example is the safe and efficient cutting of food products such as bread, meat or cheese. In every cutting machine used in commerce, crafts and industry, the aim is to precisely control the contact pressure of the relevant food product in the machine. This is made possible by the PLC, integrated in all
NORDAC frequency inverters
from NORD. It allows to freely programme drive-based control functions. This ensures consistent cutting quality.
Intelligent control functions master industry-specific drive applications
When it comes to bottling liquid food products, speed is an essential factor. NORD frequency inverters ideally meet the great demands on precise speed control. They thus ensure an optimally balanced production process. Furthermore, for example, the
NORDAC PRO control cabinet inverter
can be integrated via Ethernet. It thereby allows for the remote maintenance of the system. Online tools can thus be used to check components for errors and to evaluate any recorded data of the frequency inverter. This way, NORD ensures high system reliability.
Drive solutions from NORD also take effect when it comes to precise positioning tasks. Here, the company offers its integrated POSICON module, which, for example, is contained in frequency inverters such as NORDAC PRO. It allows automatic positioning control for different applications such as travelling theatre sceneries for trouble-free theatre performances.
Extensive modular range of products meets industry expertise
Solution provider NORD DRIVESYSTEMS develops and manufactures
application-specific drive systems from a single source
. For that, the company is using its industry expertise with which it supports
customers in about 100 industries
. The extensive range of
modular product
s, consisting of gear units, motors and electronic drive technology, forms the basis for the implementation of solutions. The components can be assembled in a modular and optimally matched manner to create customised systems.
NORD DRIVESYSTEMS was founded in 1965 and will celebrate its 60th anniversary next year. Since the beginning of the 1980s, the company has been developing and manufacturing the NORD portfolio for electronic drive control at its site in Northern German Aurich. This comprises the frequency inverters for control cabinet installation, decentralised frequency inverters and motor starters.