News –
A North German company with tradition
NORD DRIVESYSTEMS develops, produces and sells drive technology and is one of the leading international full-service providers in the industry. The success story of NORD began in 1965 in Bargteheide near Hamburg, where the company’s headquarters are still located today.
Bargteheide, 2022-06-03
The HUB in Bargteheide comprises the production, manufacturing, mounting and service sectors. 790 employees work on site on an operating area of 57,800 m2. “We want to be the best long-term partner for our customers’ drive technology and offer competent advice, shorter delivery times and comprehensive service”, says Jutta Humbert, Managing Director of GETRIEBEBAU NORD GmbH & Co.KG.
NORD has decades of experience in developing and producing various drive solutions for more than 100 industries. The company’s range includes gear units for torques from 10 Nm up to more than 282 kNm, electric motors for power ranges from 0.12 to 1,000 kW and frequency inverters up to 160 kW. The manufacturer’s inverter solutions are available for conventional control cabinet installations as well as for decentralised and fully integrated drive units. In addition to standard drives, NORD delivers application-specific concepts and solutions for special requirements such as energy-saving drives or explosion-protected systems.